Bildeinzug in Cognex VisionPro
Dieser Anwendungshinweis (in Englisch) beschreibt die Bilderfassung mit einer IDS GigE Vision Kamera und Cognex VisionPro QuickBuild.
Install Cognex VisionPro software
Please ensure that the Cognex GigE Vision Configurator and VisionPro QuickBuild are installed completely on your system.
You can find the download for the latest version of Cognex VisionPro software at the following link: http://www.cognex.com/Support/VisionPro/Software.aspx
Please consider that this software is not for free. Therefore, a valid license is required to run the software after the trial period has expired. For more information on this topic please contact Cognex.
Camera configuration via Cognex GigE Vision Configurator
After installing the VisionPro Software launch the Cognex GigE Vision Configurator Tool to assign IP addresses to your network adapter and your GigE Vision camera.
A detailed users guide can be found under the following link: https://www.cognex.com/support/downloads/File.aspx?d=815
Start VisionPro Quick Build
As far as the camera is configured correctly, you can open it in Cognex VisionPro QuickBuild in order to start the image acquisition.
Run the Cognex VisionPro QuickBuild as admin (right-click on the desktop icon and select "Run as administrator").
Open the IDS GigE Vision camera in VisionPro Quick Build
In Cognex VisionPro QuickBuild, select the image source by double clicking on the corresponding entry.
Camera configuration required!
Note that Cognex VisionPro QuickBuild requires a previously saved configuration in UserSet1 when opening a camera! Otherwise the creation of the "Image Acquisition Device" will fail. Therefore, you have to save a suitable configuration in UserSet1 on your camera in advance. This can be done very easily using the IDS Vision Cockpit. See the techtip "Line scan mode with one click" for a detailed explanation of how to use the user sets.
Select the connected IDS GigE Vision camera as "Image Acquisition Device".
Click on the "Initialize Image Acquisition" button to set the camera properties and initialize the image acquisition.
Start the image acquisition
Return to the Job Editor and acquire image.